Introduction - Johnson Controls - LIT-1201668 - System Integration - LonWorks Integration - 12.0

LonWorks Network Integration with Network Engines and LCS Technical Bulletin

Brand
Johnson Controls
Product name
LonWorks Integration
Document type
Technical Bulletin
Document number
LIT-1201668
Version
12.0
Revision date
2022-08-30
Product status
Active
Language
English

The LonWorks® Control Server (LCS) 85 is certified for use with either the Echelon® Configuration Server or the Loytec Configuration Server. The Gesytec Easylon IP Interface resides on the LCS85 and requires different settings depending on which configuration server the LCS85 uses. Other configuration servers may work with the LCS85, but are not supported by Johnson Controls.

Follow the instructions in this appendix to ensure successful operation of your LCS85. To review complete configuration procedures for each configuration server:
  • Click Help > Contents in the Echelon LonWorks/IP Configuration Server window.
  • Go to www.loytec.com and download the L-IP User Manual.