About this task
The Loytec Configuration Server is embedded in the Loytec L-IP router and can be enabled or disabled. Only one router may have the configuration server enabled.
Procedure
- Open the Windows Internet Explorer web browser.
- Enter your assigned IP address in the URL. The Loytec Device Info screen appears.
- Select Config from the vertical menu on the left.
- Log in with the administrator password to access the Loytec Config Server. If you are using firmware prior to Release 4.0, the default administrator password is admin. If you are using firmware at Release 4.0 or later, the default administrator password is loytec4u.
-
Select IP from the vertical menu on the left. The Config
IP screen appears.
Figure 1. Config IP
-
Configure the settings shown in Figure 1. See Table 1 for the options to select. Some settings vary on a per-site basis and must be modified accordingly. The IP settings are unique to your computer.
Table 1. Config IP Settings Field
Selection or Entry
DHCP/BOOTP
Disabled
IP Address
Modify accordingly.
IP Netmask
Modify accordingly.
IP Gateway
Modify accordingly.
Hostname
Modify accordingly.
Domainname
Modify accordingly.
DNS Server 1
Modify accordingly.
DNS Server 2
Modify accordingly.
DNS Server 3
Leave empty.
NAT Address
Leave empty.
MAC Address
Select Use Factory Default check box.
Link Speed & Duplex
Auto Detect
Multicast Address
Leave empty.
Connection Keep Alive
Disable
- Click Save Settings.
-
Click EIA-852 Device in the menu on the left. The Config
EIA-852 Device screen appears (Figure 2).
Figure 2. Config EIA-852 Device
-
Configure the settings shown in Figure 2. See Table 2 for the options to select. Some settings vary on a per-site basis and must be modified accordingly. The Config server address and Config server port settings are unique and cannot be used by any of the devices defined in the members list. The Config client port setting must match all devices defined in the members list.
Note: An encryption warning message may appear when you are configuring the settings. You can ignore this message. This behavior is typical for LonWorks protocol. Most sites do not require encryption.
Table 2. Config EIA-852 Device Settings Field
Selection or Entry
Config server address
Modify accordingly.
Config server port
Default is 1629. Modify accordingly.
Config client port
Default is 1628. Modify accordingly.
Device name
Modify accordingly.
Escrow timeout [ms]
Modify accordingly.
Aggregation timeout [ms]
8 (Must match the Aggregation setting in the Easylon IP Interface.)
MD5 authentication
Default is off. Enable for authentication.
MD5 secret
Leave empty unless MD5 authentication is on.
Location string
Modify accordingly.
- Click Save Settings.
-
Click EIA-852 Server in the menu on the left. The Config
EIA-852 Server screen appears (Figure 3).
Figure 3. Config EIA-852 Server
-
Configure the settings shown in Figure 3. See Table 3 for the options to select. Some settings vary on a per-site basis and must be modified accordingly. The server is enabled on only one device. All others are disabled.
Table 3. Config EIA-852 Server Settings Field
Selection or Entry
Config server status
enabled
Config server port
Default is 1629. Modify accordingly.
Channel name
Modify accordingly.
Pri.SNTP server
Leave empty.
Sec.SNTP server
Leave empty.
Channel timeout [ms]
Leave empty.
Auto members
off
Roaming members
off
MD5 authentication
Default is off. Enable for authentication.
MD5 secret
Leave empty unless MD5 authentication is on.
- Click Save Settings.
-
Click EIA-852 Ch. List in the menu on the left. The
Config Channel List screen appears (Figure 4).
Note: This screen is only available on the device that is enabled to be the configuration server.Figure 4. Config Channel List
- Click Add Device.
- Enter the device name, IP address, and port in the open fields.
- Click Save.
- Repeat Steps 15 through 17 for each device. Each device name in the list updates after the IP address and port are entered and saved. A successfully configured system has a green check mark in the Stat column.
-
See Table 4 to determine the status of your devices. Systems that do not have a green check mark do not function correctly. If necessary, see Troubleshooting communication between the configuration server and devices.
Table 4. Device Status on Loytec Config Server Icon
Status
Description
Unregistered
The ANSI/CTA-852 device is not registered with the IP-852 channel.
Not Contacted
The ANSI/CTA-852 device has not been contacted since the configuration server has started.
Registered
The ANSI/CTA-852 device is successfully registered with the IP-852 channel and is fully functional.
Not Responding
The ANSI/CTA-852 device is registered, but it is not responding at the moment.
No Extended NAT
The ANSI/CTA-852 device does not support the extended NAT mode. This device is disabled.
Disabled
The ANSI/CTA-852 device is disabled, or rejected, on the channel.
- When the configuration is complete, go to Configuring LonWorks interfaces and complete all steps in that section.