Supported Quantity of Sensors Per Controller - Johnson Controls - LIT-12011795 - LN-SVSENH-0G - LN-SVSENH-0 - LN-SVSEN-0 - LN-SVSEN-0G - Bulb controller - LN Series Communicating Sensor

LN Series Communicating Sensors Installation Instructions

Product
Network and Communications > Lonworks Networks > LN Series Communicating Sensor
Document number
LIT-12011795
Revision date
01/01/2013

LN VAV/VVT and LN-PRGxxx-12 controllers support between 4 and 12 LN Communicating Sensors. See Table 1 for the maximum allowable sensors per controller. You must set the Subnet ID of all sensors within the address range listed in Table 1.

Table 1. Number of LN Communicating Sensors Controller Models Support
Controller Series Maximum Number of Sensors Subnet ID Address Range
LN-VAV/VVT 4 1–4
LN-PRG203-12 4 1–12
LN-PRG300-12 12 1–12
LN-PRG4x0-12 12 1–12
LN-PRG6x0-12 12 1–12