About the Subnetwork Bus - Johnson Controls - LIT-12011795 - LN-SVSENH-0G - LN-SVSENH-0 - LN-SVSEN-0 - LN-SVSEN-0G - Bulb controller - LN Series Communicating Sensor

LN Series Communicating Sensors Installation Instructions

Product
Network and Communications > Lonworks Networks > LN Series Communicating Sensor
Document number
LIT-12011795
Revision date
01/01/2013

For the LN-SVSENx-0, the subnetwork bus extends the LON trunk to the LN-SVSENx-0 sensor to provide network access for maintenance and troubleshooting.

The LN-PRG6x0-12 controllers use the subnetwork bus to support the LN-IOE4x0-0 Series Modules through 2-wire shielded cable.

All LN-VAVCF-12 controllers also use the subnetwork bus to support up to four LN-SVSENx-0 sensors using standard structural cabling.

For an overview depiction of a subnetwork including LN Communicating Sensors, see Figure 4.