Location Considerations - Johnson Controls - LIT-12011795 - LN-SVSENH-0G - LN-SVSENH-0 - LN-SVSEN-0 - LN-SVSEN-0G - Bulb controller - LN Series Communicating Sensor

LN Series Communicating Sensors Installation Instructions

Product
Network and Communications > Lonworks Networks > LN Series Communicating Sensor
Document number
LIT-12011795
Revision date
01/01/2013

Do not install the device on an exterior wall, or near a heat source, air discharge grill, or where the sun can affect the sensor’s operation.

Note: The LN Communicating Sensors are not designed for outdoor use.