Updating building metadata - Johnson Controls - LIT-12012585 - Software Application - Johnson Controls Enterprise Management

Johnson Controls Enterprise Management: Professional Productivity Tool Guide

Brand
Johnson Controls
Product name
Johnson Controls Enterprise Management
Document type
User Guide
Document number
LIT-12012585
Revision date
2019-11-21
Language
English

You can update building metadata in compliance with Johnson Controls Enterprise Management requirements.

Johnson Controls Enterprise Management requires that buildings have a certain data set of building metadata. Select a building in the Located In ontology tree and enter its metadata at the bottom of the Ontology Trees pane.
Table 1. Metadata fields
Field Data type
Address1 (text)
Address2 (text)
City (text)
State Code (text)
Postal Code (number)
Timezone (drop-down selection)
Latitude (number between -90 and 90)
Longitude (number between -180 and 180)
Weather Station (drop-down selection)
Weather Station Radius (units)
  • You can use an online map service to acquire the coordinates of a building. Right-click any location on the map to obtain the GPS coordinates (latitude and longitude). Enter the coordinate data manually. If you use copy and paste, you may introduce unnecessary characters.
  • The Weather Station list becomes available after you enter the Latitude and Longitude metadata. This list contains all National Oceanic and Atmospheric Administration (NOAA) weather stations within a 50 mile radius of the coordinates. Select an appropriate weather station from the drop-down list.
  • You can copy and paste building metadata from one building to another, which is useful if there are multiple buildings at the same location. After pasting the metadata, you can adjust the GPS coordinates of the building as necessary. To copy and paste metadata, right-click on a building and select Copy Building Properties, and then right-click on another building and select Paste Building Metadata Properties.