Installation - Johnson Controls - LIT-12012585 - Software Application - Johnson Controls Enterprise Management

Johnson Controls Enterprise Management: Professional Productivity Tool Guide

Brand
Johnson Controls
Product name
Johnson Controls Enterprise Management
Document type
User Guide
Document number
LIT-12012585
Revision date
2019-11-21
Language
English

Do not mix builds of PPT, Windows Operating System, and Microsoft SQL Server Software. They must all be either 32-bit or 64-bit. It is best to use 64-bit configurations for projects on sites that contain more than 100,000 data points.

Before you install the Professional Productivity Tool on your device, you must have the following software:
  • Windows 7 Professional, Enterprise, or Ultimate Editions with SP1, or Windows 10
  • Microsoft SQL Server versions 2012, 2014 or 2016, in either Express or Full Editons.
    Note: System Configuration Tool (SCT) (at release 12) no longer supports SQL 2008 R2 (32-bit or 64-bit). We recommend that you install a later SQL Server as a separate instance, where possible.
  • Microsoft. NET 4.5
  • Microsoft Visual Basic Power Packs (part of the install package)
  • Microsoft Excel®