Checking reports on units and enumerations - Johnson Controls - LIT-12012585 - Software Application - Johnson Controls Enterprise Management

Johnson Controls Enterprise Management: Professional Productivity Tool Guide

Brand
Johnson Controls
Product name
Johnson Controls Enterprise Management
Document type
User Guide
Document number
LIT-12012585
Revision date
2019-11-21
Language
English

About this task

You can identify points that do not have the correct unit of measure or enumeration type for their point type requirements in Johnson Controls. To identify these points, you can check the units and enumeration from the Action menu. In some cases, the units of measure are incorrect in the Johnson Controls system; in other cases the system connects to the wrong point. Update the units or contact Level 1 support for more assistance. In some cases, Level 1 support may refer you to Level 2 support for further assistance with Enumeration issues.

To check that the units and enumeration are correct, complete the following steps:
  1. Click Action in the top left of the pane.
  2. Click Create Units and Enum Report.
  3. Click Save.
  4. Enter the correct enumeration type for your points in the Excel spreadsheet, if they are not correct.
  5. Click Points Without or Wrong Units tab at the bottom of the Excel spreadsheet.
  6. Enter the correct units of measure for your points in the Excel spreadsheet, if they are not correct.
  7. Click Save.

For more information about units and enumerations, see Enumeration Groups and Supported Units of Measure . Next, you can transfer data between the Professional Productivity Tool and Johnson Controls Enterprise Management.