You can create a Professional Productivity Tool Backup file of your project.
About this task
It is good practice to create project database backups in the Professional Productivity Tool. You can use these to share work with other users or recover work from a backup file. It is a good idea to create an Assessment Backup after you complete the assessment summary in the Professional Productivity Tool.
To create a PPT Project Backup file, complete the following steps:
Procedure
- From the File menu, select Create PPT Project Backup.
- Select Assessment Backup in the pop-up to save a backup in the project Assessment Backup folder.
- Click Create.
Results
Next, you can enable Commissioning Mode to view the Equipment Area pane and the Ontology trees tab at the same time.