Downloading files from JEM to your computer - Johnson Controls - LIT-12012585 - Software Application - Johnson Controls Enterprise Management

Johnson Controls Enterprise Management: Professional Productivity Tool Guide

Brand
Johnson Controls
Product name
Johnson Controls Enterprise Management
Document type
User Guide
Document number
LIT-12012585
Revision date
2019-11-21
Language
English

Procedure

  1. Log into JEM with administrator rights and select SetUp and Auto Configuration.
  2. Select the required Data Collector and Data Source.
  3. Click the Download button for each of the three files [Download file for PPT], [Download JEM Template] and [Download Data Source].
  4. Close the UI window when the spinning icon no longer displays.

Results

These files will be created in your computer users Downloads folder. Make a note of the names along the bottom of the JEM UI window, and the time that you downloaded them, so that you can find them again in the Scrub Tool.
Note: In this section, <Portfolio> is the current name of your portfolio in JEM
Table 1. Files downloaded to your computer
Files Purpose
<Portfolio>.CSV Contains a list all the Data Collectors and Data Sources in your Portfolio. This file is used by PPT later during the Export phase.
<Portfolio>.xlsx

Actual JEM configuration data. This is processed by the Scrub tool to create a file to be used by PPT.

JEMTemplateFile.xlsx

The current JEM equipment template file. May be used later by PPT to update a modified JEM configuration.

Note: Often there will be numbers like (1), (2) or (12) etc. at the end of the file name. This is a feature of Windows to allow you to download files without having an intermediate prompt to change the file name. These numbers are ignored by the Scrub Tool.