Appendix E: Scrub Export Tool Help File - Johnson Controls - LIT-12012585 - Software Application - Johnson Controls Enterprise Management

Johnson Controls Enterprise Management: Professional Productivity Tool Guide

Brand
Johnson Controls
Product name
Johnson Controls Enterprise Management
Document type
User Guide
Document number
LIT-12012585
Revision date
2019-11-21
Language
English

The purpose of the Scrub Export Tool is to clean up the JEM export files, especially for manually configured sites for JEM. The clean up of JEM export files will allow projects to be imported into PPT to create a new project.

The JEM export files includes everything available in JEM for the entire Portfolio, with one exception that only points associated with the Data Collector/Data Source are included. JEM does not identify the Locations directly and, for various reasons, JEM cannot currently provide a file with only Data Collector/Data Source equipment information. Nor can it provide complete Space and FQR information. It is expected that the export files will be in their present form at least until JEM 2.0 has been released. This is a way to pre-process before the import into PPT.