Changing Application Requirements - Johnson Controls - LIT-12012585 - Software Application - Johnson Controls Enterprise Management

Johnson Controls Enterprise Management: Professional Productivity Tool Guide

Product
Building Automation Systems > Building Automation Systems > Johnson Controls Enterprise Management
Document type
User Guide
Document number
LIT-12012585
Revision date
2019-11-21

About this task

To change the application requirements, complete the following steps:

Procedure

  1. Select Change Application Requirements from the Project Settings menu.
  2. Select the primary configuration type for your project. If your project has buildings with different configuration types, for example, Single Duct AHUs and VAVs, select the configuration type that is most common on your site. You can then use Ignore Application Requirement and set column in scope features that load from the POXOP application file.
  3. Select the Manual Selection tab. This tab displays all applications and features that load from the POXOP application file.
    Figure 1. Changing Application Requirements - manual selection

  4. You can check or clear individual features.
  5. Click Close when you complete your changes.

Results

Next, you can change trend requirements in PPT.