Application Requirements - Johnson Controls - LIT-12012585 - Software Application - Johnson Controls Enterprise Management

Johnson Controls Enterprise Management: Professional Productivity Tool Guide

Brand
Johnson Controls
Product name
Johnson Controls Enterprise Management
Document type
User Guide
Document number
LIT-12012585
Revision date
2019-11-21
Language
English

You can view and modify the default application requirements for your Professional Productivity Tool project with the Change Applications Requirements option in the Project Settings Menu. There are two tabs available in the Change Application Requirements window. You can select the primary configuration type for your project with the Q&A Selection option. You can view all applications and features that load from the POXOP application file with the Manual Selection tab.

Changes that you make on either of these tabs alter the points that the PPT Project requires, which gives the logic that determines which cells contain green or red backgrounds.

You can save modifications to a profile and export the changes to a zip file, which you can share with others or load into other Professional Productivity Tool projects.