Description - Johnson Controls - LIT-1924210 - Electric Actuator - J Series Electric Zone Valves for Assembly in the Field

J Series Electric Zone Valves for Assembly in the Field Catalog Page

Product
Document number
LIT-1924210
Revision date
2019-10-22
Figure 1. J Series Electric Zone Valve

J Series Electric Zone Valves accurately control the flow of saturated steam, hot water, and chilled water through coils and heat exchangers of all types, in a wide range of HVAC applications. The spring-return, two-position design with synchronous motor has proven reliable in millions of installations worldwide. The actuator can be removed from the valve quickly and easily, simplifying installation and servicing. No special linkage kit or commissioning is required.

Refer to the J Series Zone Valves Product Bulletin (LIT-977282) for important product application information.