The Analog outputs have a defined behavior when the values measure by the transmitter are outside the scaled analog output range.
- The output is clipped at the end of the range.
- The output is set to the error state when the measured value is 5% outside of the scaled range.
- The output resumes normal function when the measured value is back on the scaled range.