Analog Output Overrange Behavior - Johnson Controls - 24-9647-10 - Hx-68P3 Series Outside Humidity and Temperature

Hx-68P3 Series Outside Humidity and Temperature Transmitters Installation Guide

Brand
Johnson Controls
Product name
Hx-68P3 Series Outside Humidity and Temperature
Document type
Installation Guide
Document number
24-9647-10
Document revision
B
Revision date
2021-04-08
Language
English

The Analog outputs have a defined behavior when the values measure by the transmitter are outside the scaled analog output range.

  • The output is clipped at the end of the range.
  • The output is set to the error state when the measured value is 5% outside of the scaled range.
  • The output resumes normal function when the measured value is back on the scaled range.