Pole Mounting - Johnson Controls - 24-9647-10 - Hx-68P3 Series Outside Humidity and Temperature

Hx-68P3 Series Outside Humidity and Temperature Transmitters Installation Guide

Product
Network and Communications > Humidity Transmitters > Hx-68P3 Series Outside Humidity and Temperature
Document number
24-9647-10
Document revision
B
Revision date
2021-04-08

About this task

Important: We recommend a pole diameter of 2-11/32 to 3-3/32 in. (25 to 60 mm) if you use the supplied clamp and screws.

To mount the Hx-68P3 Series Outside Humidity and Temperature Transmitter to a pole:

Procedure

  1. Attach the clamp to the pole with the set screw. See Figure 6.
  2. Align the transmitter mounting bracket with the holes on the clamp, and insert the screws through the holes of the transmitter mounting bracket and into the clamp.
    Figure 1. Pole Installation

  3. Tighten the screws securing the transmitter assembly onto the pole.
  4. Plug in the screw terminal block (terminal screws facing the transmitter cover), close the cover, and tighten the cover screws. See Figure 5 for plugging in the terminal block and attaching the cover.
  5. Secure the cable to the pole using cable ties. Incorporate a drip loop below the cable gland to prevent water from running into the transmitter along the cable.
    Figure 2. Securing Cable to a Pole