Installing the Conduit Adaptor - Optional - Johnson Controls - 24-9647-10 - Hx-68P3 Series Outside Humidity and Temperature

Hx-68P3 Series Outside Humidity and Temperature Transmitters Installation Guide

Product
Network and Communications > Humidity Transmitters > Hx-68P3 Series Outside Humidity and Temperature
Document number
24-9647-10
Document revision
B
Revision date
2021-04-08

About this task

Using the conduit adaptor is optional. If you do not use the conduit adaptor, proceed to Mounting .

To install the conduit adaptor, follow these steps.

Procedure

  1. Loosen the six captive screws that hold the transmitter cover in place. See Figure 5.
  2. Unscrew the cable gland from the transmitter cover. See Figure 1 for the location of the cable gland.
  3. Align the nut with the opening inside the transmitter cover, and insert the adaptor body into the transmitter conduit opening.
    Figure 1. Conduit Adaptor

  4. Manually tighten the adaptor into the nut, turning in a clockwise direction.
  5. Tighten the adaptor onto the adaptor body, turning in a clockwise direction.