The DIP switches on the component board control the humidity output parameter and scaling. Figure 3 shows the default DIP switch settings.
Change the position of the DIP switches to the desired setting.
| DIP Switch Position | Analog Output Parameter and Scaling |
|---|---|
|
|
Relative Humidity (RH)0 to 100%Temperature (T)-40 to 60°C |
|
|
Dewpoint (Td)-40 to 60°CTemperature (T)-40 to 60°C |
|
|
Enthalpy (h)-40 to 460 kJ/kgTemperature (T)-40 to 60°C |
|
|
Wet Bulb Temperature (Tw)-40 to 60°CTemperature (T)-40 to 60°C |
| DIP Switch Position | Analog Output Parameter and Scaling |
|---|---|
|
|
Relative Humidity (RH)0 to 100%Temperature (T)-40 to 140 ° F |
|
|
Dewpoint (Td)-40 to 140°FTemperature (T)-40 to 140°F |
|
|
Enthalpy (h)-10 to 190 BTU/lbTemperature (T)-40 to 140°F |
|
|
Wet Bulb Temperature (Tw)-40 to 140°FTemperature (T)-40 to 140°F |