DIP Switch Settings - Johnson Controls - 24-9647-10 - Hx-68P3 Series Outside Humidity and Temperature

Hx-68P3 Series Outside Humidity and Temperature Transmitters Installation Guide

Brand
Johnson Controls
Product name
Hx-68P3 Series Outside Humidity and Temperature
Document type
Installation Guide
Document number
24-9647-10
Document revision
B
Revision date
2021-04-08
Language
English

The DIP switches on the component board control the humidity output parameter and scaling. Figure 3 shows the default DIP switch settings.

Figure 1. DIP Switch Positions

Change the position of the DIP switches to the desired setting.

Table 1. DIP Switch Positions for Metric Output
DIP Switch Position Analog Output Parameter and Scaling

Relative Humidity (RH)0 to 100%Temperature (T)-40 to 60°C

Dewpoint (Td)-40 to 60°CTemperature (T)-40 to 60°C

Enthalpy (h)-40 to 460 kJ/kgTemperature (T)-40 to 60°C

Wet Bulb Temperature (Tw)-40 to 60°CTemperature (T)-40 to 60°C

Table 2. DIP Switch Positions for Non-Metric Output
DIP Switch Position Analog Output Parameter and Scaling

Relative Humidity (RH)0 to 100%Temperature (T)-40 to 140 ° F

Dewpoint (Td)-40 to 140°FTemperature (T)-40 to 140°F

Enthalpy (h)-10 to 190 BTU/lbTemperature (T)-40 to 140°F

Wet Bulb Temperature (Tw)-40 to 140°FTemperature (T)-40 to 140°F