Application Requirements - Johnson Controls - 24-9647-10 - Hx-68P3 Series Outside Humidity and Temperature

Hx-68P3 Series Outside Humidity and Temperature Transmitters Installation Guide

Product
Network and Communications > Humidity Transmitters > Hx-68P3 Series Outside Humidity and Temperature
Document type
Installation Guide
Document number
24-9647-10
Document revision
B
Revision date
2021-04-08

The Hx-68P3 Series Outside Humidity and Temperature Transmitter measures and transmits outside relative humidity (RH) from 0 to 100% and temperatures from -40 to 140°F (-40 to 60°C). In addition to RH, the transmitter offers selectable parameters including dew point, wet bulb temperature, and enthalpy.

The integral weather shield provides ventilation, blocks direct and reflected solar radiation, and blocks precipitation without affecting performance. Mount the transmitter outside on a pole or on a side of a building.

Important: The Hx-68P3 Series Outside Humidity and Temperature Transmitter is intended to provide an input to equipment under normal operating conditions. Where failure or malfunction of the humidity and temperature transmitter could lead to personal injury or property damage to the controlled equipment or other property, additional precautions must be designed into the control system. Incorporate and maintain other devices, such as supervisory or alarm systems or safety or limit controls, intended to warn of or protect against failure or malfunction of the humidity and temperature transmitter.
Important: Le Hx-68P3 Series Outside Humidity and Temperature Transmitter est destiné à transmettre des données entrantes à un équipement dans des conditions normales de fonctionnement. Lorsqu'une défaillance ou un dysfonctionnement du humidity and temperature transmitter risque de provoquer des blessures ou d'endommager l'équipement contrôlé ou un autre équipement, la conception du système de contrôle doit intégrer des dispositifs de protection supplémentaires. Veiller dans ce cas à intégrer de façon permanente d'autres dispositifs, tels que des systèmes de supervision ou d'alarme, ou des dispositifs de sécurité ou de limitation, ayant une fonction d'avertissement ou de protection en cas de défaillance ou de dysfonctionnement du humidity and temperature transmitter.