Description - Johnson Controls - LIT-1900867 - Humidity Transmitter - Hx-68P3 Series Outside Humidity and Temperature Transmitters

Hx-68P3 Series Outside Humidity and Temperature Transmitters Catalog Page

Product
Network and Communications > Humidity Transmitters > Hx-68P3 Series Outside Humidity and Temperature Transmitters
Document number
LIT-1900867
Revision date
2020-10-16

The Hx-68P3 Series Outside Humidity and Temperature Transmitter measures and transmits outside relative humidity (RH) from 0 to 100% and temperatures from -40 to 140°F (-40 to 60°C). In addition to RH, the transmitter offers selectable parameters including dew point, wet bulb temperature, and enthalpy.

The humidity sensor is impervious to dust and most chemicals and is not damaged by condensation. The weather shield protects the sensors from solar radiation and precipitation without affecting performance. The multiple discs have a unique profile that permits easy passage of air. The disc material is especially formulated for high reflectivity, low thermal conductivity and maximum weather resistance. This rugged enclosure will assure a long life, even under extreme weather conditions.

The sensor and shield function as one unit for optimal performance. Mount the transmitter outside on a pole or on a side of a building. It requires no routine maintenance or recalibration.

Refer to the Hx-68P3 Series Outside Humidity and Temperature Transmitters Product Bulletin (LIT-12011896) for important product application information.

Figure 1. Hx-68P3 Series Outside Humidity and Temperature Transmitter