Before installation, configure the element for the required output signal. See Figure 1 to set the output jumper for the application.
Figure 1. Output jumper setting
| Number | Description |
|---|---|
| 1 | 0 VDC to 5 VDC |
| 2 | 0 VDC to 10 VDC |
| 3 | Probe |
Note: The factory setting is No. 2.