Introduction - Johnson Controls - GS3CALKIT - Gas Detection Sensor - GS3000 CO or NO2 Calibration Kit

GS3000 CO or NO2 Calibration Kit GS3CALKIT

Product
Sensors and Meters > Carbon Dioxide Devices > GS3000 CO or NO2 Calibration Kit
Document revision
A
Revision date
2021-04-01
Part number
24-11484-00048

The GS3CALKIT is a kit to correctly calibrate the GS3000 Gas Detection Sensor Series. The GS3CALKIT includes:

  • Tubing
  • Regulator
  • Calibration cap 1 (GS3000)
  • Calibration cap 2 (GS3000 Indoor)
  • Carrying case
  • Sponge, for CO only
Note: Calibration gas is not included, purchase this locally.

Calibration gas requirements, 103 liter tanks:

  • 250 ppm CO in air
  • 10 ppm NO2 in air
Figure 1. GS3CALKIT