1 |
Access media tray including Cortana, settings,
notifications, Wi-Fi signal strength, volume, and brightness |
2 |
The indoor temperature and relative humidity in the
space |
3 |
Total energy savings for the last 7 days, select for
daily detail |
4 |
Indicates when voice command is enabled and allows the
microphone to be muted and un-muted |
5 |
The current outdoor temperature, forecast, and the
highs and lows for the day based on your postal code with Wi-Fi
connection |
6 |
View and edit your current schedule |
7 |
See your current indoor and outdoor air quality based
on measurements tVOC, eqCO2, allergens, AQI, UV index, and
relative humidity |