1 |
Access media tray including Cortana, settings,
notifications, Wi-Fi, volume, and
brightness |
2 |
Device keeps the space at the Home setpoints,
depending on the schedule |
3 |
Auto
mode will heat and cool automatically to stay
within the selected setpoints |
4 |
Heat
mode will heat to stay within the selected
setpoints |
5 |
The
fan will run automatically when heating or
cooling |
6 |
Indicates when voice command is enabled and
allows the microphone to be muted and
un-muted |
7 |
Device keeps the space at the Away
setpoints |
8 |
Off
mode will keep your heating and cooling system off
unless safety features are enabled and the heat or
freeze protection temperatures are reached |
9 |
Cool
mode will cool to stay within the selected
setpoints |
10 |
Manually power on fan for air circulation with optional runtimes of 15
minutes, 30 minutes, 1 hour, 2 hours, 4 hours, and Stay On |