If the FAC/IOM control panel assembly fails to operate within its specifications, replace the unit. For a replacement assembly, contact the nearest Johnson Controls® representative.
Quantity | Description |
---|---|
1 |
Metal Enclosure, Type 1 with slotted flush latch and perforated sub-panel, enclosure not included with sub-panel assembly |
1 |
MS-FAC4911-0 digital controller, which operates on BACnet/IP networks |
1 |
MS-IOM4711-0 (if applicable) |
1 |
96 VA 120/24 VAC power supply with 5 A primary circuit protection and two 120 VAC outlets (standard on all panels) |
1 |
96 VA 120/24 VAC transformer with secondary protection (if applicable) |
1 |
Five- or ten-point 24 VAC distribution terminal block |