Description - Johnson Controls - LIT-1921670 - T-4054m - Room Thermostat - Pneumatic Thermostat - Energy Manager Heating-Cooling High Volume Output Thermostat

Energy Manager Heating-Cooling High Volume Output Thermostat Catalog Page

Product
Thermostats > Pneumatic Thermostats > Energy Manager Heating-Cooling High Volume Output Thermostat
Document number
LIT-1921670
Revision date
2020-01-08

The T-4054 Heating-Cooling, Energy Manager Thermostat is a high volume output, with an adjustable deadband of 0 to 30°F (0 to 16°C) between heating and cooling set points.

Refer to T-4000 Series Pneumatic Room Thermostat Product Bulletin (LIT-7171060P) for important product information.

Figure 1. T-4054 Heating-Cooling, Energy Manager Thermostat