Mounting - Johnson Controls - DP140 - Differential Pressure Transducer - DP140 Series Differential Pressure Transducer

Differential Pressure Transducer DP140 Series Installation Guide

Product
Switches and Electrical > Differential Pressure Transducers > DP140 Series Differential Pressure Transducer
Document type
Installation Guide
Document revision
Revision date
13/05/2021
Part number
24-11486-00012

The DP140 transducer includes 3/16 in. O.D. barbed brass pressure fittings, installed with 1/4 in. push-on tubing. For the shortest response times, use 3/16 in. I.D. for tubing lengths up to 100 feet long, 1/4 in. I.D. for tubing lengths up to 300 feet, and 3/8 in. I.D. for tubing lengths up to 900 feet. The static positive pressure port, labelled High, is located on the bottom of the unit. The reference pressure port, labelled Low, is located on the bottom of the unit. Use the reference pressure port for differential pressure measurements.