About this task
Wiring is through a 1/2 in. threaded conduit opening. Both current and voltage output units are reverse wiring protected.
Note: Figure 1 shows the voltage
output and Figure 2 shows the
current output, both for electrical code 1.
Important: For voltage outputs, do not connect +Excitation to +Out/Sig as
this results in unrecoverable damage to the board.
To install the DP140 transducer, complete the following steps: