This procedure allows you to mass edit attributes of online controllers at once.
-
From the Tools menu, select Trunk Utilities > Read/Write Attributes Online. The Trunk Utilities - Read/Write Attributes wizard appears with the Connection screen active.
-
Select the desired connection type and parameters and click Next. The Attribute Template screen appears.Note: We strongly advise against using an Supervisor Passthru connection to transfer to multiple controllers due to potential communication loss during the process.
-
Click Discover to begin the discovery process and locate devices. When devices are located, they appear in the main section of the Attribute Template screen.
Note: To stop the Discover process, click Stop. -
Select the devices from the list.
Note: If more than one device has the same Instance Number, the numbers display red in the device list. -
Perform the following tasks:
-
To browse for an existing attribute template file, click the Browse button. Navigate to the location of the template and click Open.
-
To save a template, click the Save button. Navigate to the correct directory, enter a file name, and click Save.
-
To add a new device, click the Add button (+).
-
To remove a currently selected device, click the Remove button (-).
-
To change the device name within the template, click in the field that contains the existing template name and enter a new name.
Note: The device name and instance number are only written during a transfer to device process. These values cannot be written during a read/write operation. -
To add a new attribute, click the Click To Define New Attribute column heading. A tree representation of the application appears. Choose the module, element, and attribute from the tree and click OK. The parameters are added to the template and appear as a column on the screen.
Note: To add a new attribute, you must have a CAF open before you select Read/Write Attributes. -
To remove an existing attribute, right-click the heading and select Remove Attribute.
Note: The Discovered column indicates whether the device is added due to device discovery. -
To manually change the Device Address or Instance Number for discovered devices only, edit the field value.Notes:
- To auto assign the device address of every device in the Instance Number column, right-click the Instance Number heading and click Auto Assign.
- To assign instance number values to devices based on the device number, trunk number, and device address, right-click the Instance Number heading and click Assign Calculated Instance.
-
-
To pull current values from the selected devices, click Read Attributes.
-
To make changes to the values found, use the drop-down menu to select the desired value or edit the field value.
-
Click Write Attributes. The updated attributes are sent back to the devices.
-
Click Copy To Clipboard to copy and paste the data from the template to another word-processing program, such as Microsoft Notepad.
-
Click Save to retain any changes you made to the attribute template. The Save dialog box appears.
-
Click Save.
-
When modifications are complete, click Finish. The wizard closes.