Trunk Utilities - Transfer Controller CAFs to Computer Wizard - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

Table 1. Trunk Utilities - Transfer Controller CAFs to Computer Wizard

Field

Description

Connection Screen

Connection Type

Use to specify the connection type to use:

  • Supervisor Passthru

  • Bluetooth

  • MAP 4.2+/BACnet Router

  • ZigBee

Connection Parameters

Supervisor Passthru: Use to specify the following:

  • Host name/IP Address: Indicates the device host name or IP Address.
  • Username and Password: Indicates the user name and password to log in to the site.
Note: The Supervisor Passthru fields allows you to connect directly to a site by entering in the site's user name and password.
  • Supervisor Device: Displays a list of discovered supervisory devices.
  • Trunk: Displays a list of trunks for the selected supervisory device.

Bluetooth: Use to specify the COM port and baud rate to use.

MAP 4.2+ / BACnet Router: Use to specify the following:

  • IP address and UDP port of the router.
  • Network number of the MS/TP trunk (1-65,534).
    Note: Do not use 1001 for the MS/TP Network Number. The MS/TP Network Number 1001 is reserved for Johnson Controls IP network connections.
  • An available Ethernet network interface adapter to use.
    Note: If you select an available Ethernet network interface, all IP traffic intended for the MAP 4.2+/ BACnet Router travels through this interface.
When you first open the wizard, the default connection parameters for connecting to a MAP Gateway at version 4.2 are automatically displayed. If the connection parameters are modified, the values are stored in the wizard for future use. To restore the connection parameters to the default values, click the MAP 4.2 Default button.
Note: For further information about the MAP and common troubleshooting issues, refer to the Mobile Access Portal Gateway User's Guide (LIT-12011999).

ZigBee: Use to specify the Personal Area Network (PAN) Offset.

Transfer to Computer Screen

Directory to Save Files to Computer Text Box and Browse Button

Use to browse to and select the desired directory in which to transfer the device CAFs to the computer. The selected directory appears in the field.

Browse Button

Use to select the directory and file name of the transfer template file.

Save Button

Prompts you to browse for a directory and type a file name to save the transfer template file.

Devices Table

Available devices, including:
  • Selected: Indicates if the device is selected (selected box) or not selected (empty box).
  • Discovered: Indicates if the device is added due to device discovery (selected box) or added from a template (empty box).
  • Name: Name of the device.
  • Model: Indicates the model number of the device.
  • Main Code Version: Indicates the Main Code version in the device.
  • Boot Code Version: Indicates the Boot Code version in the device.
  • Device Address: MS/TP device address.
  • Instance Number (BACnet ID): BACnet ID of the device.
    Note: If more than one device has the same Instance Number, the numbers display red in the device list.
  • Status: Indicates the status of the transfer to computer operation after the Finish button is selected.

View Status Button

Opens the Status dialog box showing the current status of the operation. Click Refresh periodically to update the status. Click Copy To Clipboard to copy and paste the text to another word-processing program, such as Microsoft Notepad.

View Log Button

Opens the Log dialog box showing the detailed operation log file. Click Refresh periodically to update the log. Click Copy To Clipboard to copy and paste the text to another word-processing program, such as Microsoft Notepad.

Clear Log Button

Clears all contents of the log file.

Get Device Info Button

Use for devices imported from a transfer template (the transfer template does not store the device model or the boot and Main Code versions). The Get Device Info button retrieves the boot and Main Code values from the actual device so an transfer to the controller can be properly done.

Discovery Button

Starts the Discovery process for locating devices.

Stop Button

Stops the Discovery process.

Navigation Buttons

Previous

 

Clear Log Button

Clears all contents of the log file.

Get Device Info Button

Use for devices imported from a transfer template (the transfer template does not store the device model or the boot and Main Code versions). The Get Device Info button retrieves the boot and Main Code values from the actual device so an transfer to the controller can be properly done.

Discovery Button

Starts the Discovery process for locating devices.

Stop Button

Stops the Discovery process.

Navigation Buttons

Previous

 

Next

Moves to the next screen of the wizard.

Finish/Done

Finish starts the transfer to the computer.

Done appears after the transfer to the computer completes. Click Done to close the wizard.

Cancel

Closes the wizard without performing the transfer.

Opens the Help system.