If you use the Transfer CAF and Attributes to Controller option through Trunk Utilities, the application files are transferred to controllers in parallel. This is more efficient than the serial application file transfer to controllers in the Transfer CAFs to Multiple Controllers option.
Field |
Description |
---|---|
Connection Screen |
|
Connection Type |
Select the type of connection to use:
|
Connection Parameters |
Supervisor Passthru: Specify the following:
Note: The Supervisor Passthru fields allows you to connect directly to a
site by entering in the site's user name and password.
|
Bluetooth: Specify the COM port and baud rate to use. Product Type radio buttons allows you to choose a communication parameter between Metasys or Facility Explorer based controller products. |
|
MAP 4.2+ / BACnet Router: Use to specify the following:
When you first open the wizard, the default connection parameters for connecting
to a MAP Gateway at version 4.2 are automatically displayed. If the connection
parameters are modified, the values are stored in the wizard for future use. To
restore the connection parameters to the default values, click the MAP 4.2
Default button.
Note: For further information about the MAP and common
troubleshooting issues, refer to the Mobile Access Portal Gateway User's
Guide (LIT-12011999).
|
|
ZigBee: Specify the Personal Area Network (PAN) Offset. Product Type radio buttons allows you to choose a communication parameter between Metasys or Facility Explorer based controller products. |
|
Connected - Attribute Template Screen |
|
Browse Button |
Select the directory and file name of the attribute template file. |
Save Button |
Browse for a directory and type a file name to save the attribute template file. |
Devices Table |
Available devices, including:
|
Read Attributes Button |
Reads current values from the selected devices. |
Write Attributes Button |
Writes updated attributes back to the devices. |
Copy to Clipboard Button |
Copies and pastes the text to another word-processing program, such as Microsoft Notepad. |
Discovery Button |
Starts the Discovery process for locating devices. |
Stop Button |
Stops the Discovery process. |
Transfer Screen |
|
Browse Button |
Select the directory and file name of the transfer template file. |
Save Button |
Browse for a directory and type a file name to save the transfer template file. |
Force Main Transfer Check Box |
Force a Main Code transfer to controller. If this check box is not selected, the Main Code is transferred to the device only if the code is different. If the check box is selected, the Main Code is always transferred to the device. |
Force Boot Transfer Check Box |
Select to force a Boot Code transfer to the device. If this check box is not selected, the Boot Code is never transferred to the device. If this check box is selected, the Boot Code is always transferred to the device. |
Devices Table |
Available devices, including:
|
View Status Button |
Opens the Status dialog box showing the current status of the operation. Click Refresh periodically to update the status. Click Copy To Clipboard to copy and paste the text to another word-processing program, such as Microsoft Notepad. |
View Log Button |
Opens the Log dialog box showing the detailed operation log file. Click Refresh periodically to update the log. Click Copy To Clipboard to copy and paste the text to another program, such as Microsoft Notepad. |
Clear Log Button |
Clears all contents of the log file. |
Get Device Info Button |
Use for devices imported from a transfer template (the transfer template does not store the device model or the boot and Main Code versions). The Get Device Info button retrieves the boot and Main Code values from the actual device so a transfer to the device can be properly done. |
Discovery Button |
Starts the Discovery process for locating devices. |
Stop Button |
Stops the Discovery process. |
Navigation Buttons |
|
Previous |
Moves to the previous screen of the wizard. |
Next |
Moves to the next screen of the wizard. |
Finish/Done |
Click Finish to start the transfer. Click Done to close the wizard. |
Cancel |
Closes the wizard without performing the transfer. |
|
Opens the Help system. |