Working with the Trunk Utilities - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

The Trunk Utilities allow you to perform a transfer to a computer or device and upgrade multiple devices on the same trunk at once, as well as mass edit attributes of multiple devices on the same trunk using attribute templates.

To transfer to the computer or transfer to a single device, see the Transfer Operations section. For information on upgrading a CAF or using the Bulk CAF Upgrade Utility, see the Upgrading System Files section.