VAV Subordinate Single Duct Applications - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

For single duct subordinate applications, no zone temperature or setpoint logic is created. Instead, Network Input points read corresponding values using peer-to-peer references from the associated Master VAV application to track key Mode states, inputs for CO2 and OA Percent, Flow Status and % Command, and any heating outputs from the master VAV box. Using this technique to control the VAV subordinates ensures that the manager and subordinate boxes are synchronized to heat and cool the entire space.