Temperature (VAV-SD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
All applications require a zone temperature sensor. This input defaults to a SAB signal to use a net stat and not consume additional IO points. The Setpoint Adjust option allows you to choose either Common Setpoint Adjust or a Warm Cool Adjust. You may also optionally select to add Temp Occ Support to include an input for temporary occupancy requests.