Discharge Air Temperature (VAV-SD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

This option is used primarily as a commissioning check-out feature for applications that have Box Heating to ensure the Discharge Air Temperature increases when Box Heating is commanded on. Discharge Air Temperature is also used when Discharge Air Reset by Zone Control is selected in the Box Reheat Coil Control section.