Power Fail Restart Logic (VAV-SD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

This feature is available as part of the Unit Enable Determination State Generator module. When this option is selected, after a restart (power cycle, transfer to the controller, or manual restart command), the application is held in the shutdown state for the Power Fail Restart Time (default = 60 seconds).