This option allows the unit to shut down based on the energy hold off Network Input. If Energy Hold Off Switch is selected in the Misc (VAV-SD) section, then the Network Input or the Hardware Input (BI) can activate the mode. This feature is typically used to shut down the temperature and airflow control when a window or loading door is open (for example, a window switch).