Occupancy (VAV-SD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The Always Occupied option sets the default value of Occupied for the ZN-T Setpoint Determination and Balancer Override modules to Occupied. Select this option if the space is occupied continuously or if shutdown is preferred to unoccupied mode.

The Scheduled Occupancy creates the interface for the Supervisory system scheduling logic. Select this option if the space changes mode based on a scheduled input. The Override Support option creates a software point that supersedes the Occupancy Schedule as well as local interfaces, such as optional Occupancy Sensors or Networked Sensor Temporary Occupancy.