The selection options for the Sensors/Inputs are:
-
Discharge Air Temperature: This option is used primarily as a monitoring feature during commissioning.
-
Zone (always required): A Zone Temperature Input is always provided. All the Zone Temperature options assume that a model of the Network Sensor family is being used for Temperature, the Setpoint Adjust options of Common Setpoint Adjust or Warm Cool Adjust, a Temporary Occupancy Interface from the Network Sensor, and Humidity input from the Network Sensor. Refer to the Network Sensors product literature to match the functionality selected for the application with a specific Network Sensor hardware model. See the ZN-T Setpoint Determination section for details on how this module works.
-
Temperature
-
Setpoint Adjust
-
Common Setpoint Adjust
-
Warm Cool Adjust
-
-
Temp Occ Support
-
-
Humidity
-
Occupancy: This option provides an Input interface to the logic from a separate Occupancy Sensor.
-
CO2 Sensor: This option provides an Input interface to the logic from a separate CO2 Sensor.
-
Used for Minimum Flow Reset
-
-