VAV Master and Subordinate Dual Duct Peer References - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

Table 1 summarizes all of the possible Network Inputs created in the VAV Subordinate Dual Duct Applications and their corresponding Peer References to read from the Master VAV application.

Table 1. VAV Master and Subordinate Dual Duct Peer References

Subordinate Application Network Inputs

Master Application Object ID Type and Name

Master Object ID Peer Reference

AUTOCAL-C

Autocal State value from the Autocalibration Sequence (Autocalibration Sequence v50) State Generation module

MV 3091

CD-OA%

Network Input

CD-OA%

AV 10

EMERGENCY-MODE

Smoke Sequence-State value from the Smoke Control Sequencing for UL-864-UUKL State Generation module

MV 3915

HD-OA%

Network Input

HD-OA%

AV 36

MSTRCDFLOW-OUTSTATE

CDD-OUTSTATE parameter from the CD Damper Control module

MV 3123 (Constant Flow)

MV 3126 (Variable Flow)

MSTRCDFLOW-PERCENT

Damper % Command value from the CD Damper Control module

AV 78370 (Variable Flow)

AV 78241 (Constant Flow)

MSTRHDFLOW-OUTSTATE

HDD-OUTSTATE parameter from the HD Damper Control module

MV 3224 (Constant Flow)

MV 3226 (Variable Flow)

MSTRHDFLOW-PERCENT

Damper % Command value from the HD Damper Control module

AV 78628 (Variable Flow)

AV 78499 (Constant Flow)

MSTRSUPHTG1-C

Electric On Off

Output

SUPHTG1-C

BO 2126

MSTRSUPHTG1-C

Steam/Hot Water On Off

Output

SUPHTG1-C

BO 2128

MSTRSUPHTG-O

Incremental

Output

SUPHTG-O

AO 2129

MSTRSUPHTG-O

Proportional

Output

SUPHTG-O

AO 2127

MSTRZN-CO2

Input

ZN-Q

AI 1100