You can access both the online Controller Tool Help and the PDF to quickly find information. The tool supports context-sensitive help, which provides you with instant access to a help topic from a component in the user interface. However, in some instances, such as when searching with multiple keywords, the PDF provides the better option for finding information. To open a PDF of the help file, select Topics PDF in the Help menu.