Printing Summary Reports - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

About this task

For information on printing the logic diagram, see Printing the Logic Diagram in the Configuring a System section.

To print a summary report of the information in the tool:

Procedure

  1. On the File menu, select Print. The Summary Report Options dialog box appears.
  2. Select the check boxes for the information you want to print. See the Summary Report Options screen section for descriptions.
  3. Click OK. The tool creates a PDF using Adobe® Reader® software containing the selected information in report format.
    Note: If the Summary Report does not open in Adobe Reader software, see the workaround in the Troubleshooting section.
  4. Print or save the PDF as desired from the Adobe Reader software.