Commissioning - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

Commissioning mode allows you to connect to a device and view actual data from that device. You can use this mode to monitor your device and set Offsets, COVs, and Polarity in addition to other Parameter and Detail changes. For example, you can change the Min Out and Max Out values of an Output to fine tune the range of a 2 to 10 VDC proportional valve. In addition, the Commissioning mode has a balancing feature for VAV applications to easily autocalibrate VAV boxes and set flow constants in one location. See the Commissioning a System section.

Back to Modes