Controller Application File (CAF) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

A Controller Application File (CAF) is a file which contains all the logic components needed to represent a system. The tool prompts you to save a controller application file for each system you create. Saving this file allows you to access it again later to make changes or to use it for additional systems.

The default location to save a CAF is C:\Users\<username>

You cannot use certain characters when saving a CAF. Invalid characters include:

: * ? " < > | / \