Logic View Status Colors - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

Table 1 lists the status colors used in the Logic View.

Table 1. Logic View Status Colors

Status Color

Appears in Mode

Description

Yellow Block

All modes

Indicates an activity input.

Turquoise Block

All modes

Indicates an activity output.

Tan Block

All modes

Indicates a block that contains logic that you can edit.

White Block

All modes

Indicates a block that does not contain logic you can edit.
Note: The Hybrid Activity State block is white with the selected state highlighted in blue.

White Block with Blue State

All modes

Indicates a Hybrid Activity State block.

Block with Yellow Input

All modes

Indicates a connected input.

Block with Orange Input

All modes

Indicates an input that is not connected.

Block with Green Input

All modes

Indicates an input available for connection from the selected block.

Black Block

All modes

Indicates the default element of a module/block.

Black Line

All modes

Indicates a regular connection line.

Black Line with Red Circle

All modes

Indicates the connection units or enumeration sets do not match.

Blue Line

All modes

Indicates a selected connection line.

Magenta Line

All modes

Indicates connections traced by the selected block.

Yellow Circle

All modes

Indicates a hidden edge label connected to an input.

Gray Circle

All modes

Indicates a hidden edge label connected to something other than an input.

(Advanced Item: Alarm, Trend, or Schedule)

All modes

Identifies a block that has an alarm, trend, or schedule defined.