Network Outputs - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The Network Outputs category appears in the Control tab (Figure 1). This section lists the network outputs defined for the system. A network output module acts as a network variable read from a supervisory device. When a network output is not mapped to a supervisory device, it uses its default value. During Simulation and Commissioning modes, a network output may be commanded. Network outputs connect from other modules or the State Table.

During Simulation and Commissioning modes, the Network Outputs category displays a second row of text. This row provides the Network Outputs present value.

See Network Output Modules for information. Also, see Peer-to-Peer Communication in the Configuring a System for information on peer-to-peer communication in the tool.

Back to Control Tab Module Categories