Control Tab Module Categories - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

The module categories are the sections of the Control tab representing the main items that make up a system (for example, the Network Inputs and Network Outputs sections). The modules in the sections are automatically added based on the items selected for your system in the System Selection Wizard. For information on this wizard, see the System Selection Wizard in the Configuring a System section.

The module category sections in the Control tab are:

See Figure 1 for the location of these categories on the UI.