System Upgrade (without Modules) Screen - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

See Upgrading a System.

Table 1. System Upgrade (without Modules) Screen

Field

Description

Yes

Closes the System Upgrade screen and upgrades the CAF.

No

Closes the System Upgrade screen and does not upgrade the CAF.

Help

Opens the Help system.